Technical FAQs

Ask a Question

What is the duty cycle for the Altivar ATV18 braking?

Issue: What is the duty cycle for the Altivar ATV18 braking?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: A 50 % duty cycle is what it is rated for.


 
Was this helpful?
What can we do to improve the information ?