Technical FAQs

Ask a Question

What are the repair parts for a SC816F150CH Series M01?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
Meter Cover - 40561-678-50
Load Center Cover - 40561-575-50
Dead Front Cover - 40561-737-01
Load center interior (breaker base) - 40561-617-51
Meter Base assembly - 40561-900-50
Meter Jaw - 40527-069-50 (OBSOLETE - REPLACED BY 73297-948-50)
Meter Jaw Blade Guide - 40527-619-01
Fifth Jaw Assembly - 40527-295-50
Line side horn bypass (2) - 40561-509-01
Left load side horn bypass - 40527-831-01
Right load side horn bypass - 40527-831-02
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2590
Was this helpful?
What can we do to improve the information ?