Technical FAQs

Ask a Question

Why can`t we get commissioning terminal part number PP01 (remote keypad) to work on Omegapak 8803?

Need to confirm if the unit is a constant torque or variable torque unit because keypad only works on constant torque units.

CTA-ID : 4037
Was this helpful?
What can we do to improve the information ?