Technical FAQs

Ask a Question

What size speed potentiometer should be used with the Omegapak 8803 unit?

You can use a 2.5kohm 1/2 watt potentiometer.
For Example: part number 9001K2007(5KOhm). This is a 30 mm type K operator and POT.
Another option is the ATVPOT25K(2.5KOhm). This is a 22 mm POT.


CTA-ID : 4033
Was this helpful?
What can we do to improve the information ?