Technical FAQs

Ask a Question

What is the fuse replacement that is mounted on top of the Omegapak 8803 unit?

The fuse is a FARRAZ, HOM RS6. If this fuse is mounted on top of the unit then it should be an 8803 drive that came from Europe. We do not supply that fuse because it does not meet UL requirements. Need to contact point of purchase.

CTA-ID : 4026
Was this helpful?
What can we do to improve the information ?