Technical FAQs

Ask a Question

Can ground-fault alarm be used on a Micrologic circuit breaker without PowerLogic?

Yes. Bulletin 0502DB0001 describes the components and wiring necessary to use a full-function Micrologic circuit breaker with the GF alarm option (trip unit function ``A``.

CTA-ID : 2805
Was this helpful?
What can we do to improve the information ?