Technical FAQs

Ask a Question

What are the repair parts for a QMB362H, Series D2 (D02)?

Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4051239950
Load Base Assembly (1 required, includes lugs) - 4051241150
Load Base Mounting Screw (1 required per load base) - 2142717161
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101652
Lug Mounting Nut - 2342501701




CTA-ID : 2842
Was this helpful?
What can we do to improve the information ?