Technical FAQs

Ask a Question

What are the repair parts for a SC816F150S Series M01?

Issue:
Previous Design Repair Parts

Product Line:
Combination Service Entrance Devices

Environment:
Repair parts

Cause:
Maintenance

Resolution:

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056171950
Meter Cover Mounting Screw - 4020513002K (This kit contains 10 screws, but only two screws are required to secure the cover)
Utility Pullbox Cover - 4056194450 (Includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056194250 (Includes hinges)
Load Center Cover Mounting Screws - (2) 2142217101
Dead Front Interior Trim - 4056192301
Dead Front Interior Trim Mounting Screw - 4020513002K (This kit contains 10 screws, but only two screws are required to secure the interior trim)
Load Center Interior - 4056188350 (Does not include main breaker)
Load Center Interior Mounting Screw - (2) 4020510001, (1) 4020511201 and (2) 4020516101 (3`` Long Wire Guide Screws)
Load Center Line Bussing Insulating Shield - 4056171401
Load Center Line Bussing Insulating Shield Mounting Screw - 4020513002K (This kit contains 10 screws, but only two screws are required to secure the insulator)
Main Breaker - QOM2150VH
Meter Base - 7329882750 (Base only - does not include jaws, see below)
Meter Base Mounting Screw - (2) 2142717200
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850)
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Meter Sealing Ring - 2920910001
Line Side Phase Lug - (2) 4025116051
Line Side Phase Lug Mounting Keps Nut - (2) 2342702001
Line Side Neutral Lugs are not field repairable.
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

 
Was this helpful?
What can we do to improve the information ?