Technical FAQs

Ask a Question

Can the output current on the 8803 be adjusted using the pc software option?

Yes, the output can be chosen from the local control in the software menu.


CTA-ID : 4008
Was this helpful?
What can we do to improve the information ?