Technical FAQs

Ask a Question

What are the repair parts for a CU12L400N Series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
Meter Cover - 40561-731-50
Load Center Cover - 40561-361-52
Utility lug cover(Pullbox) - 40561-729-01
Dead Front Cover - 40561-537-01
Load center interior (breaker base) - 40545-227-50
Meter Base Assembly - 21324CD
Mounting Channel - 40561-420-03
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2561
Was this helpful?
What can we do to improve the information ?