Technical FAQs

Ask a Question

What are the repair parts for a C200RB series MO1?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
Meter Cover - 40534-141-50
Load Center Cover - 40534-492-50
Dead Front Cover - 40534-436-01
Hinges for Load center cover - X2983
Load center interior (breaker base) - 40545-012-03
Meter Base Assembly - 40534-484-50
Meter Jaw - 40527-069-50 (OBSOLETE - REPLACED BY 73297-948-50)
Meter jaw blade guide - 40527-619-01
Left line side lug - 40534-087-50
Right Line side lug - 40534-088-50
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2558
Was this helpful?
What can we do to improve the information ?