Technical FAQs

Ask a Question

What are the repair parts for a QMB362T21W, Series E1 (E01)?

The QMB device is a twin switch, meaning it contains two switches in the one device. One side is 30A, the other is 60A. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4051239950
Load Base Assembly 60A (1 required, includes lugs) - 4051241150
Load Base Assembly 30A (1 required, includes lugs) - 4051242550
Load Base Mounting Screw (2 required per load base) - 4020506501
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101652
Lug Mounting Nut (per lug) - 2342702001




CTA-ID : 3091
Was this helpful?
What can we do to improve the information ?