Technical FAQs

Ask a Question

What are the repair parts for a HOM20M100CK, Series S01 load center?

Only the parts listed below are considered field replaceable:
Cover - HOMC24UC
Cover Mounting Screw - 4020513002K
Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit 4020284450K
Interior Assembly - HOM20M100CI
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM100VH
WireGator Insert - 4055615301 (Includes 1)
WireGator Shields Kit - 4055943550 (Includes 2 shields, mounting screws and 4 slot closures)

CTA-ID : 3088
Was this helpful?
What can we do to improve the information ?