Technical FAQs

Ask a Question

What is the lenght of the capillary bulb of a 9025GXW24 ?

It is 4``l x .69``w. Additional information is available in Digest 170 or in Book 112 of the Help Files.


CTA-ID : 2814
Was this helpful?
What can we do to improve the information ?