Technical FAQs

Ask a Question

What is the combination suffix for 1212 + 1021? Can this combination be used on ME and MX type circuit breakers?

Suffix is 1380 . Yes, this suffix is acceptable for (3) pole module versions of FA/FH/FC through PA/PH/PC and Micrologic LE/LX through PE/PX types.


CTA-ID : 2797
Was this helpful?
What can we do to improve the information ?