Technical FAQs

Ask a Question

On a QO three-phase main circuit breaker or main lugs Nema 3R load center, when the cover is replaced, do the hinges come with the cover?

Yes. The hinges come with the cover on a Nema 3R three-phase load center cover.


CTA-ID : 2519
Was this helpful?
What can we do to improve the information ?