Technical FAQs

Ask a Question

QO Two Pole, 240 PL Remotely operated Circuit Breaker. What are the white, black and red wires connect to?

The black lead is connected to the negative of the power supply, the white lead is connected to the external control device and the red is connected to the positive of the power supply.


CTA-ID : 3030
Was this helpful?
What can we do to improve the information ?