Technical FAQs

Ask a Question

What are the repair parts for a QO116M100RB, Series S2, Load Center?

Issue:
Design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4056317750
Interior Trim with Labels - 4056313001K (remove main breaker knockout in the field)
Interior Assembly - QO116M100RBI
Neutral Bonding Screw - 4028345850K
Main Circuit Breaker - QOM100VH
Interior Trim Mounting Screws - 4020513001K
RB Door Mounting Screws - 2142217101
Outdoor Cover Latch - 4056314701
Outdoor Latch Rivet - 2410212160
Main Circuit Breaker and Main Lug Keps Nut - 2342702001


CTA-ID : 2780
Was this helpful?
What can we do to improve the information ?