Technical FAQs

Ask a Question

What are the repair parts for a QO11220M100C, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - QOC12UF
Interior Assembly - QO11220M100I
Neutral Bonding Screw - 4028345850K
Main Circuit Breaker - QOM100VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main Circuit Breaker and Main Lug Keps Nut - 2342702001


CTA-ID : 2776
Was this helpful?
What can we do to improve the information ?