Technical FAQs

Ask a Question

What are the repair parts for a QO112M100K, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - QOC12UF/S
Interior Assembly - QO112M100I
Neutral Bonding Screw - 4028345850K
Main Circuit Breaker - QOM100VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main Circuit Breaker and Main Lug Keps Nut - 2342702001
Wiregator Inserts - 4055615301
Wiregator Wieguard Shields - 4055943550, QTY 2


CTA-ID : 2773
Was this helpful?
What can we do to improve the information ?