Technical FAQs

Ask a Question

What are the repair parts for a QO124L125GK, Series S1?<br />

Only the parts listed below are considered field replaceable.
Cover - QOC24UF/S
Interior Assembly - QO124L125GI
Neutral Bonding screw - 4028345850K
Main Lugs - QOL125
Indoor Cover mounting screw - 4020513002K
Indoor Cover Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main circuit breaker and main lugs keps nut -2342702001
Wiregator Inserts - 4055615301
Wiregator Wireguard Shields - 4055943550, QTY 2



CTA-ID : 2503
Was this helpful?
What can we do to improve the information ?