Technical FAQs

Ask a Question

Is it necessary to adjust the Micrologic factory settings?


Issue:
What to I set my settings at on micrologic trip unit

Product Line:
Circuit Breakers

Environment:
Applies to micrologic trip units, legacy type trip units as well as new micrologic trip units.

Cause:
What do I set settings at  on micrologic trip unit? How do I determine trip unit settings?

Resolution:
The settings for circuit breaker with micrologic trip units should be determined by a coordination study, or if not applicable, by the bus it needs to protect and the requirements of the electrical system.


CTA-ID : 3023
Was this helpful?
What can we do to improve the information ?