Technical FAQs

Ask a Question

CK type MG breaker. Is the T at the end of the trip unit for ground fault?

Yes, T at the end of the trip unit is for ground fault.


CTA-ID : 2770
Was this helpful?
What can we do to improve the information ?