Technical FAQs

Ask a Question

What are the repair parts for a QC2040M200C Series M01?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
meter cover - 40561-678-50
load center cover - 40561-575-50
Deadfront (interior Trim) - 40561-736-01
load center interior - 40561-618-50
meter base assembly - 40561-901-50
meter jaw - 40527-069-50 (OBSOLETE - REPLACED BY 73297-948-50)
meter jaw blade guide - 40527-619-01
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2758
Was this helpful?
What can we do to improve the information ?