Technical FAQs

Ask a Question

Can commercially available no-ox grease be used to grease the plug-on jaws of an I-line breaker?

Absolutely not. Commercially available greases will cause a poor connection to the bus and possible damage to the electrical equipment. The only thing that can be used on the jaws is the PJC-7201 joint compound listed in the Supplementary Digest.


CTA-ID : 2469
Was this helpful?
What can we do to improve the information ?