Technical FAQs

Ask a Question

What does AIR mean?

AIR means ``Ampere Interrupting Rating.`` It is the maximum short-circuit current a circuit breaker can safely interrupt at a given voltage.
It replaces the former designation of AIC which stood for ``Ampere Interrupting Capacity.``


CTA-ID : 2480
Was this helpful?
What can we do to improve the information ?