Technical FAQs

Ask a Question

What are the repair parts for a QO140M225, Series S01 (or S1), Load Center?

Issue:
Design repair parts

Product line:
QO load centers

Environment:
Repair parts

Cause:
maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - QOC42UF/S
Interior Assembly - QO140M225I
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2225VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit 4020284450K
Main Circuit Breaker and Main Lugs Keps Nut - 2342702001


CTA-ID : 3259
Was this helpful?
What can we do to improve the information ?