Technical FAQs

Ask a Question

What are the repair parts for a SU3040D400B Series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
Meter Cover - 4056173150
Load Center Cover - 4056136152
Utility Pullbox Cover - 4056172901 (Does not include handles, see below)
Utility Pullbox Cover Handles - (2) 2940101103, Handle Mounting Screws (8) 2142217101
Deadfront (Interior Trim) - 4056131003
Load Center Interior - 4055842550
Meter Base Assembly - 21324CD
Mounting Channel - 4056142003
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2743
Was this helpful?
What can we do to improve the information ?