Technical FAQs

Ask a Question

Do all CM UL listed AC voltage shunt trips operate at 55% of rated voltage?<br />

Yes. All CM UL listed AC voltage shunt trips operate at 55% of voltage. DC voltage shunt trips operate at 75% of rated voltage.
See technical manual (AC0036/3E page 12).


CTA-ID : 2459
Was this helpful?
What can we do to improve the information ?