Technical FAQs

Ask a Question

Can a breaker trip if the handle is locked into the ON postion?

Yes. All MCCBs are trip-free devices. This is a requirement of UL489.


CTA-ID : 3253
Was this helpful?
What can we do to improve the information ?