Technical FAQs

Ask a Question

When ordering an SE breaker with ground fault is the neutral CT ordered separately?

Yes, this is true for LX, LE, MX, ME, NX, NE, PX, PE, NX, NE and SE


CTA-ID : 2640
Was this helpful?
What can we do to improve the information ?