Technical FAQs

Ask a Question

Have a FA34080. Is there a 250 amp version.

FA only goes to 100A. For 250A, go up to the next frame size: KA36250.


CTA-ID : 2438
Was this helpful?
What can we do to improve the information ?