Technical FAQs

Ask a Question

Does Schneider Electric offer ambient compensated circuit breakers?

Issue:
Selection, Application

Product Line:
Circuit Breakers

Environment:
UL489, NFPA 70

Cause:
Circuit protection may be required in circumstances for which the anticipated ambient temperature is very high or very low.

Resolution:
No, there is not an adjustment option for ambient temperature. For ambient temperatures outside of the 25 to 40 deg. C range, use the re-rating charts in document # 0100DB0101 available here.


CTA-ID : 2417
Was this helpful?
What can we do to improve the information ?