Technical FAQs

Ask a Question

Arc Fault breaker (AFI) 1P 15A what does it do?

It is a UL listed circuit breaker which is also classified for mitigating the effects of arcing faults. It protects from arcs between hot and neutral (above 50A), and arcs between hot and ground.


CTA-ID : 3220
Was this helpful?
What can we do to improve the information ?