Technical FAQs

Ask a Question

Is it possible to defeat, turn off, or otherwise remove the ground-fault feature from an LE, LX, or LXI type circuit breaker with a Micrologic Series B trip unit?

No. The ground fault function can be minimized by setting the pickup and delay to maximum.

CTA-ID : 2700
Was this helpful?
What can we do to improve the information ?