Technical FAQs

Ask a Question

What would the catalog number be to factory install a 24Vac shunt trip and one auxiliary switch on a NJHF36000S60 Compact NSJ molded case switch?

You must add the two digit suffix numbers at the end of the NSJ catalog number for the accessories. The two digit suffix for a 24Vac shunt trip is ``SK``. The two digit suffix for one auxiliary switch is ``AA``. According to proper catalog number construction, the auxiliary suffix must go before the shunt trip suffix. Therefore the complete catalog number would be NJHF36000S60AASK.


CTA-ID : 2697
Was this helpful?
What can we do to improve the information ?