Technical FAQs

Ask a Question

Can ground fault be added in the field to a NXL361200?

No, adding ground fault to a non-ground fault NX breaker is not possible. The breaker must be ordered with the option present--NXL361200G.


CTA-ID : 2678
Was this helpful?
What can we do to improve the information ?