Technical FAQs

Ask a Question

What are the repair parts for a QMB335W, Series E1 (E01)?

Only the parts listed below are considered field replaceable:
Arc Suppressor Assembly (3 per switch) - 4052028950
Load Base Assembly (3 per switch, includes lugs) - 4052054750
Load Base Mounting Screw (3 required per load base) - 2142720241
Load Base Side Insulator (1 per load base) - 4052098601
Handle Knob Kit - 4028343550
Lug Assembly - must order load base assembly

CTA-ID : 3191
Was this helpful?
What can we do to improve the information ?