Technical FAQs

Ask a Question

What is the magnetic setting range for the old Multi 9 ``U`` curve?

The U curve magnetic setting operated between 5.5 and 8.8 times ampere rating. None of the existing C60N Multi 9 curves have this exact value. The closest is the C curve at 7 and 10 times ampere rating.


CTA-ID : 2926
Was this helpful?
What can we do to improve the information ?