Technical FAQs

Ask a Question

Can two wires per phase be terminated on the KC34250?

No, only one wire per phase is possible with the KC, KI, KA, KH breakers


CTA-ID : 2925
Was this helpful?
What can we do to improve the information ?