Technical FAQs

Ask a Question

What is the Omegapak 8804 service bulletin part number 8804-50 March 1990 Serial Communications Option Baord corrections that have been made according to the errata sheet 0001?

Three pages of the manual were updated and the following changes made: Page 25: Table 5.2 drive address switch settings have been corrected, Page 39: Register 0004 - Acceleration time must be greeater than the acceleration (not deceleration) pote


CTA-ID : 4096
Was this helpful?
What can we do to improve the information ?