Technical FAQs

Ask a Question

What is the Omegapak 8804 service bulletin part number of the Types MC30 ( PT-Mod H08; VT-Mod H07; part number 52011-548-53 { drive run relay }), MC31 ( PT-Mod G08; VT-Mod G07; part number 52011-548-52 { non-isolated input }), MC32 ( PT-Mod F08; VT-Mod F0 )?

8804-52 is the part number of the manual.


CTA-ID : 4094
Was this helpful?
What can we do to improve the information ?