Technical FAQs

Ask a Question

What are the repair parts for a QMB264W, Series E1 (E01)?

Only the parts listed below are considered field replaceable:
Arc Suppressor Assembly (2 required per switch) - 4052028950
Load Base Assembly (2 per switch, includes lugs) - 4052002550
Load Base Mounting Screw (2 required per load base) - 4020506501
Load Base Side Insulator (1 per load base) - 4052025201
Handle Knob Kit - 4028343650
Lug Assembly (per lug) - 4025116251
Lug Mounting Nut (per lug) - 2342702200




CTA-ID : 3173
Was this helpful?
What can we do to improve the information ?