Technical FAQs

Ask a Question

What are the repair parts for a QO13040L200GK, Series S1, Load Center?<br />

Only the parts listed below are concidered field replaceable.
Cover - QOC30UF/S
Interior Assembly - QO13040L200GI
Neutral bonding screw - 4028344850K
Main Lugs - QOL225
Indoor cover mounting screw - 4020513002K
Indoor cover hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main circuit breaker and main lugs keps nut - 2342702001
Wiregator Inserts - 4055615301, QTY 2
Wiregator Wireguard shields - 4055943550

CTA-ID : 2639
Was this helpful?
What can we do to improve the information ?