Technical FAQs

Ask a Question

Is the following part 52011-002-01 still available for the Omegapak 8804?

The proper updated part number for the gate driver board is 52011-003-50 which is what the number represented,


CTA-ID : 4077
Was this helpful?
What can we do to improve the information ?