Technical FAQs

Ask a Question

Why will the Omegapak 8804 not run in hand or auto?

Need to check wiring. Try jumping 34 to 44 and 2 to 14 and make sure 3-22 and 41-42 are jumped. These jumpers isolate the control wiring and then can isolate issue which suspect is a wiring problem if verify there are no faults.

CTA-ID : 4073
Was this helpful?
What can we do to improve the information ?