Technical FAQs

Ask a Question

Why could the Omegapak 8804 unit be tripping on undervoltage and won`t reset?

Check the 24VAC on pins 23 and 24 of the MCB on the drive, which is the voltage the drive uses to detect undervoltage. If it is above 20.5VAC then it is probably a MCB problem and it should be replaced.

CTA-ID : 4071
Was this helpful?
What can we do to improve the information ?