Technical FAQs

Ask a Question

Which full fuction LE, LEL, PEF breakers are not 100% rated?

The 600 amp sensor in the LE, LEL and the 2500 amp sensor in the PEF are 80% rated.


CTA-ID : 3072
Was this helpful?
What can we do to improve the information ?