Technical FAQs

Ask a Question

What are the repair parts for a QO12030M150C, Series S1 (or S01) Load Center?

Issue:
Design repair parts

Product Line
QO load centers

Environment
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable.
Cover - QOC30UF
Interior Assembly - QO12030M150I
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2150VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main Circuit Breaker and Main Lugs Keps Nut - 2342702001


CTA-ID : 2878
Was this helpful?
What can we do to improve the information ?