Technical FAQs

Ask a Question

Do Square D float switches have any differential to prevent frequent switching as tank levels change ?

No. Mounting the float in a protected well within the tank may help. Also consider interposing an Off delay timer per M178D on Telegraphing Pilot Devices. Depending on the severity of the movement, an On delay timer may also be needed.


CTA-ID : 2638
Was this helpful?
What can we do to improve the information ?